All-in-One IDMS for Enhanced Grid Resilience and Customer Satisfaction
The complexity and huge quantities of data that smart grids generate require transformational control room solutions. The integrated distribution management system (IDMS) gives operators a holistic view with advanced optimisation analytics, helping them make better operational and business decisions.

Radical, transformative technologies often start out by imitating the old school solutions they replace. The “horseless carriages” of the late 19th and early 20th centuries kept many features of horse-drawn vehicles. A similar phenomenon can be seen in the electricity industry. On a simple consumer level, you can buy a light bulb that looks (a bit) like a flickering candle. At the extremely complex level of network control, digital technologies were inspired by analogue systems.
An analogue control room is almost a work of art. The centerpiece is a large map-board of the distribution network that covers the walls. Operators are placed around the room in such a way as to maximise their view of the paper maps, push-pins and various objects stuck onto the board to show the state of the system. Just as the first printed books were designed to look like the parchments they replaced, so a “traditional” digital distribution management system is basically a map-board on a digital screen. The operators don’t have to walk around a room any more to get an overall view of the network, but they do have to consult several screens and rely on a relatively limited amount of data to make critical real-time decisions.
Positive impacts at every level
All that has changed with the new generation of smart distribution control rooms and the introduction of integrated distribution management systems. GE Vernova's Grid Solutions' Network Management Solutions Activity Director IDMS, Dr. Avnaesh Jayantilal, is enthusiastic about the possibilities the new technologies will bring to utilities. “Our IDMS is based on our core e-terradistribution technology and has positive impacts at every level, from enhanced situational awareness, improved reactivity and enhanced safety in the field to improved reliability and operational improvement.” And all that is on “a single pane of glass” providing a comprehensive supervisory control and data acquisition (SCADA) system, distribution management system (DMS) and outage management system (OMS).
The IDMS is made up of a number of modules. The network analysis module is based on a robust distribution network power flow that supports a fully unbalanced model for both radial and meshed medium-/low-voltage networks. It analyses distribution power flow, distribution state estimation, power quality, losses, short circuits, and load modeling. This allows dispatchers and planning engineers to study the current and future state of the network.
Our IDMS is based on our core e-terra distribution technology and has positive impacts at every level.
The network module provides an enhanced level of analysis allowing the dispatcher to improve the network configuration and achieve one or more predefined objectives: for example, keeping nodal voltages and branch currents inside operational limits, maintaining power factor requirements at specific locations in the network, or reducing total demand or losses in the distribution network. It includes load and Volt/VAr optimisation (VVO), fault location, isolation and service restoration (FLISR), planned outage study (POS) and automated feeder reconfiguration (AFR).
The switching operations module interfaces directly to the network models. Switching orders can be created manually or generated automatically by the network enhancement functions. In practice, this clearly allows utilities to optimise system resources, but there are significant benefits in terms of human resources too.
A learning tool
Dr. Jayantilal also highlights the possibilities of using these capabilities of the IDMS as a learning tool. “Major storm events seem to be getting more frequent. The IDMS was developed to process high volumes of data to enhance network resiliency and restoration, but it can also simulate a major event. Utilities can prepare their employees and processes for future events, but also analyse data collected during a storm to see how to improve performance.”
The IDMS includes a state of-the-art training simulator that is able to simulate large-scale outages from major storms. The simulation includes field equipment operations, customer calls, power-on/off messages from smart meters, and crew responses.
Business process transformation
Dr. Jayantilal illustrates what this means for Stedin, which is one of the largest distribution utilities in the Netherlands, providing electricity and gas to over 2 million private, corporate and government customers, and to one of the largest ports in the world, Rotterdam. “Stedin was performing 6,000 switching orders a year, all manual and paper-based, taking about 90 minutes each. IDMS reduced the processing time to 30 minutes. Stedin was able to reassign two full-time employees to other critical duties thanks to the 6,000 hours they saved. And, by the way, the IDMS only took up one of those 30 minutes; the other 29 went to all the processing and approvals.”
Stedin also shows how digital technologies can quickly be adapted to interesting new uses. One of the key benefits of deploying the IDMS is the ability to automatically transfer relevant network and outage information in real-time through social media to communicate with customers. Stedin’s experience shows that during an outage, customer satisfaction tends to improve when customers are informed about the cause of the outage and, critically, the expected restoration time. Stedin is planning on sharing a real-time, read-only version of their IDMS with the local safety authorities to help improve coordination during major storms.
Make the most of what you’ve got
For Dr. Jayantilal, one of the most interesting benefits is that the IDMS can help utilities avoid having to invest in new capacity just to manage peak load scenarios and network congestion. “With the IDMS, utilities can better manage their medium- and low-voltage assets in the field and push them harder and closer to their real limits.” The IDMS can also perform automated network self-healing by using the FLISR application to reduce customer outage times.
On a global scale, Dr. Jayantilal also sees distributed energy resources (DERs) as a major challenge for utilities in the future, and one that GE Vernova will help utilities meet. DER growth driven by regulatory incentives and sustainability objectives has introduced both technical and commercial challenges for the utilities. On the technical side, the network analysis applications have been enhanced to incorporate complex models for DER including solar-photovoltaic, energy storage, demand response and electric vehicle charging, with new real-time dashboards for operators.
The IDMS is helping utilities all over the world make the most of smart grids. But as Dr. Jayantilal says, it’s also helping them reach a goal that hasn’t changed since the first electricity networks were built: “Provide reliable, safe and affordable electricity to their customers.”
Zoom on the outage management system
IDMS outage management system
The IDMS outage management system (OMS) module collects, coordinates and analyses outage information from customer calls, automated meter observations (AMI), and SCADA data. It assists the dispatcher by determining the most likely point at which customer supply has been lost and coordinating crews and other activities through the repair and restoration process. It is designed to handle storm situations, provide basic workcrew monitoring functionality, and calculate distribution performance indices to meet regulatory reporting requirements.
Its ability to merge historical and state-of-the-art outage observations is a huge performance benefit in large-scale events. The OMS utilises AMI observations to complement phone calls and to verify the extent of outages and, more importantly, verify complete restorations.
The system treats each customer end-point as an individual entity connected to a dynamic, as-operated wired model. As the OMS system model always reflects actual connectivity, customers are always tied to the correct energisation sources (or not, when de-energized).
The OMS does not make gross assumptions (for example, assuming a static model); hence the restoration performance and accuracy of outage reporting metrics are improved significantly. Uniquely, it recognizes and models dynamic partial restorations and abnormal energization paths. Accurately handling nested outages and partial restorations also improves the accuracy of outage performance indices. Integration with DMS modules enables automatic creation of switching orders that are validated with the network analysis applications to ensure network resilience is maintained.

Outage analysis

Switch order

Outage calls