The History of Gas-Insulated Substations
Gas-insulated substations (GIS) represent a key element of high-voltage electrical transmission networks thanks to its reliability, low maintenance requirements and compact dimensions. Here is a brief history of its development and pioneers.

[1966 - The first 245 GIS installed at Plessis-Gassot, near Paris in France]
The roots of HV encapsulated substations go back to the metal enclosed concept of the 1920s when oil was used as the insulating medium. Compressed air and different gases were the focus of much research work, and the first Freon-based solution at 33 kV appeared in 1936. The following decades brought new versions until developments in industrial processes, chemistry and physics led the switchgear industry, towards the end of the 20th Century, to the use of SF6 (Sulfur Hexafluoride) for arc extinguishing and insulation as the main GIS technology.
 SF6 gas was already known during the 1940s. Westinghouse holds the original patent for the use of SF6 as an interrupting medium, and their engineers developed the first applications for switches and circuit breakers in the early 1950s. In the 1960s major manufacturers such as BBC-Calor Emag, Siemens, Magrini, Merlin-Gerin, NEI-Reyrolle, the Japanese and Delle-Alsthom had started intensive developments on the basis of SF6. The dual-pressure SF6 circuit breakers of the early GIS systems were soon replaced by single pressure, while circuit breakers were adopting puffer and combined thermal-puffer arc extinguishing chambers. The GIS focus was on the benefits of a compact indoor solution, protected from the environment and closer to users, whereas some markets preferred outdoor rugged solutions using hybrid GIS solutions.
SF6 gas was already known during the 1940s. Westinghouse holds the original patent for the use of SF6 as an interrupting medium, and their engineers developed the first applications for switches and circuit breakers in the early 1950s. In the 1960s major manufacturers such as BBC-Calor Emag, Siemens, Magrini, Merlin-Gerin, NEI-Reyrolle, the Japanese and Delle-Alsthom had started intensive developments on the basis of SF6. The dual-pressure SF6 circuit breakers of the early GIS systems were soon replaced by single pressure, while circuit breakers were adopting puffer and combined thermal-puffer arc extinguishing chambers. The GIS focus was on the benefits of a compact indoor solution, protected from the environment and closer to users, whereas some markets preferred outdoor rugged solutions using hybrid GIS solutions.
 GE Vernova's Contribution
GE Vernova's Contribution
GE Vernova's Grid Solutions business has a rich GIS development history through its ancestor companies, Delle-Alsthom, Sprecher & Schuh, GEC, and AEG.
 
Delle-Alsthom France started GIS development in 1958 and in 1966-1967 delivered a world's first with its “Fluobloc” at 245 kV in several Paris substations, demonstrating the benefits of underground GIS to supply bulk power close to city users. Achievements in the higher voltage ranges were subsequently marked by the deliveries of the first substations for 420 kV in 1976 and for 550 kV in 1977. Another “world-first” was the completion of AEP’s 800 kV GIS in Joshua Falls in 1979.
 
Sprecher & Schuh studied compact metalclad installations as early as 1954 with oil insulation systems, but soon concluded that SF6 gas insulation offered greater advantages. Their first GIS for 220 kV was delivered in 1970 and the 145 kV, 40 kA in 1971. The original circuit breakers with double-pressure SF6 systems (220 kV, 50 kA), developed together with ITE USA, were operated by the well-known Sprecher motor-wound spring operating mechanisms, which contributed to the success of subsequent GIS families. The exclusive third-generation FK mechanism today serves all Grid Solutions' GIS products in applications around the world.
 
AEG in Germany has also long been involved in GIS and SF6, with its first GIS substation delivered in 1971.
 
Meanwhile, GEC in England was collaborating with Siemens, and their first GIS was a 145 kV substation in London in 1982. As GIS systems developed and their extensive use in HV networks grew, Grid Solutions became the manufacturer of complete GIS ranges of 72.5-800 kV in which single-phase and three-phase encapsulation was and continues to be used.
Looking ahead
Clearly, the most significant development factor was the adoption of SF6 as an insulation medium. This boosted the development of smaller switchgear requiring less operating energy and reduced materials and resources, leading to higher performance. So far 420 kV, 63 kA with a single break is possible with the spring mechanism.
After 50 years in the making, GIS development is accelerating thanks to the availability of simulation tools and the capability to integrate environmental needs into the design. Future trends could be influenced by the substitution of SF6 technology, which, however, is likely to be a very complex task. Other steps have already been taken. Moving HV substations closer to consumers results in reduced transmission losses. Indoor GIS reduce the environmental influences on the switchgear, reducing maintenance needs and increasing lifetime. More and more “intelligence” is integrated into the GIS using electronic devices, forming part of digital substations. Ecological and economic considerations, together with ongoing technological developments have made even further optimisation of GIS conceivable.

[2018 - GE Vernova's first 145 g3-GIS installed at Axpo's Etzel substation, in Switzerland]