AI and Energy: Two Infrastructures, One Future
There is a moment in every major technological shift when the supporting infrastructure stops being background context and becomes the story itself. We are at that moment now — and the infrastructure in question is energy.
AI is scaling at a pace the world has not seen before. Large AI data centers already require hundreds of megawatts of electricity. Some new campuses are approaching gigawatt-scale power demand. The challenge is no longer simply about producing enough electricity. It is about delivering that electricity reliably, efficiently, and intelligently through a power system that was not designed for this new reality.
This is not a minor adjustment. It is a fundamental rethinking of how digital and energy infrastructure must be planned, built, and operated together.
The Scale of What We Are Building
To understand what is happening, it helps to look back. About a century ago, building the electrical grid was one of the largest infrastructure transformations in human history. It required coordinated investment in power generation, transmission networks, substations, and control systems — built over decades, across continents, connecting billions of people to reliable electricity for the first time.
Today, we are witnessing something of comparable scale and ambition with AI infrastructure. It is not simply about GPUs or models. It requires an entire ecosystem — compute, networking, cooling, and power systems — working together as a single, integrated system. The industry has begun to reflect this reality through the concept of AI factories: large-scale computing environments designed from the ground up as coherent, co-engineered systems.
Reference Architectures: The Foundation for Scaling AI Infrastructure
Building something at global scale has always required a common language.
When the electrical grid was being built a century ago, the industry quickly learned that fragmented, incompatible approaches created costly inefficiencies. Over time, shared standards, common design patterns, and coordinated frameworks emerged — allowing complex infrastructure to be replicated, connected, and scaled more effectively. That hard-won standardization is a large part of why the grid became the foundational, reliable system it is today.
The same principle is now at work in AI infrastructure — and the lessons of the past are worth heeding early.
At GE Vernova, we have developed reference architectures that establish proven patterns for deploying power infrastructure at AI factory scale — providing a common starting point that helps align developers, operators, utilities, and technology providers around shared design intent. These frameworks are foundational. They reduce complexity, accelerate deployment, and bring the kind of predictability and repeatability that large-scale infrastructure demands.
But reference architectures become even more powerful when paired with the ability to test them against reality before deployment begins. This is precisely where our collaboration with NVIDIA DSX adds a critical dimension. By connecting our high-fidelity, three-dimensional digital twins of critical grid assets directly with the environments in which AI infrastructure is designed and deployed, we can evaluate how architectures behave under real operating conditions — accounting for regional grid characteristics, transient events, and evolving workload patterns.
This does not replace reference architectures. It strengthens them — bringing designs closer to the realities they will encounter once deployed and ensuring that power and compute can be engineered together with greater speed and confidence from day one.
Just as the pioneers of the electrical grid understood that generation alone was never enough (and that transmission, substations, and control systems had to work as one), we believe that the AI factories of today require the same end-to-end architectural clarity. In a world where AI progress is measured in months, that clarity is not a luxury, but a competitive necessity.
The Energy Challenge — and the Opportunity Within It
Supporting AI infrastructure at this scale requires capabilities across the entire energy value chain: power generation, transmission capacity, sustainable energy solutions, and efficient power distribution. In many regions today, grid capacity and connection timelines are already becoming key factors in how quickly large digital infrastructure can be deployed.
But here is what makes this moment genuinely different: the very technology driving demand is also becoming one of our most powerful tools for managing that demand. AI is not only increasing the load on energy systems. It is also transforming how those systems are operated.
With more sensors, richer operational data, and advanced analytics, grid operators can monitor infrastructure in near real time, anticipate failures before they occur, enhance power flows dynamically, and integrate renewable energy more efficiently. The result is a grid that can absorb complexity rather than be overwhelmed by it.
And there is another dimension worth highlighting in that AI factories themselves, when designed with the right architecture, can actively support grid stability. By dynamically adjusting power consumption and participating in grid flexibility services, they can help balance supply and demand, turning what might appear to be a pure load challenge into a two-way relationship between digital and energy infrastructure.
AI needs energy to exist and energy needs AI to transform.
Digital Twins: From Design Intent to Real-World Confidence
One of the most powerful tools emerging at the intersection of AI and energy is the digital twin.
Electric power systems are genuinely complex — combining physical infrastructure, telecommunications networks, and vast amounts of operational data that interact in ways traditional methods struggle to model. Digital twin technologies allow engineers to simulate these systems, including power networks and large compute environments, before a single piece of hardware is deployed.
This fundamentally changes the economics and timeline of infrastructure development. Instead of discovering design challenges during commissioning or early operation, teams can identify and resolve them virtually, improving designs, stress-testing control strategies, and validating performance under real-world grid conditions long before construction begins.
At GE Vernova, this means we can model and enhance the interaction between digital infrastructure and power infrastructure, helping ensure that AI factories connect to the grid efficiently, reliably, and in a way that supports rather than strains the broader energy system. The result is a shift from reactive adjustment to proactive, predictive infrastructure development.
A New Era of Infrastructure Thinking
What this moment demands is a new kind of infrastructure thinking: one that does not treat power and compute as separate domains but recognizes them as deeply, structurally interconnected.
The companies and institutions that build this understanding into their strategies early will be better positioned to deliver the performance, resilience, and speed that the AI era requires.
At GE Vernova, we are committed to being a trusted partner in this transition, bringing deep expertise in energy systems, digital technologies, and infrastructure design to help build the foundation that AI infrastructure needs to scale. Through our collaboration with NVIDIA and our contribution to the DSX ecosystem, we are helping ensure that the energy systems powering AI factories are designed with the same ambition, precision, and foresight as the compute systems they support.
The grid that powers AI and the AI that transforms the grid are not two separate stories. They are one — and we are at the beginning of writing it together.