Legacy Infrastructure is Putting a Huge Strain on the Grid. Here’s How Operators Can Take Back Control.
Aging grid infrastructure is reaching a critical breaking point. And operators are feeling it. Despite the fact that electrical demand is growing and the energy transition continues to accelerate, grid operators are still relying on assets and systems that were designed decades ago.
That disconnect between legacy capabilities and modern demands isn’t just slowing everything down. It’s leading to very real consequences — more outages, more risk, more operational drag. Read more to discover the current state of today’s aging grid, why legacy infrastructure can’t cope with projected demands, and the specific risks caused by outdated technology.
We’ll also explain how GridBeats™ Automation and Protection System (APS) can help, including how it gives operators a way to modernize from within by removing the structural complexity of aging systems.
The Grid is Getting Older Faster than Utilities Can Modernize
According to recent estimates, almost one-third (30%) of grids are now over 40 years old. By 2050, that figure could reach an estimated 90%. It’s hard to see how existing infrastructure will cope based on current trends and projections.
For instance, an American society of Civil Engineers (ASCE) report revealed that electricity peak demand growth reached its highest point in two decades in 2025, while summer and winter peak demands are forecast to rise 15% and 18% respectively by 2034.
This surge in demand is being driven by a host of factors, including the enormous energy requirements of data centers, which are predicted to demand 35 GW of electricity by 2030.
The Consequences Are Already Visible — and Escalating
Grid investments have been declining for over a decade. To illustrate the point, 70% of lines and transformers were already over 25 years old as of 2023 and spending on transmission has plummeted since the mid-2010s.
As extreme weather events continue to rise, and dated infrastructure remains in place, it’s clear that premature grid failures will become more frequent and disruptive. In fact, the same ACSE report noted that “Aging infrastructure systems are increasingly vulnerable to natural disasters and extreme weather events.”
Adding substance to that claim, a report by the U.S. Energy Information Administration revealed that U.S. customers experienced an average of 11 hours of electricity interruptions in 2024. That figure is nearly double the annual average of the previous decade, with hurricanes and extreme weather cited as major contributing factors. Grid investments have been declining for over a decade. To illustrate the point.
Why is Aging Infrastructure So Hard to Manage?
Perhaps the most obvious reason is that mechanical failures are just more likely. The limitations of aging assets also lead to network inadequacy. The consequence? More unplanned outages, rising maintenance costs, and protracted replacement cycles.
Legacy systems also create substantial operational complexity. For instance, they can be unstable during peak demand. And crucially, they weren’t built to handle bi-directional power flows — an issue that will only become more acute as we move towards a new era of renewable energy.
The Real Problem
In truth, the issues with aging grid infrastructure aren’t just related to old hardware; they’re related to structural complexity and stem from:
• Multi-vendor estates with different firmware, hardware, and update cycles
• Legacy systems that can’t integrate with new technologies
• Patchwork communication systems that provide limited real-time insight
• Manual, error-prone patching and slow upgrades
As a grid operator, you’ll likely know firsthand how these issues don’t just hinder daily tasks and communication. They introduce real risk and disruption into your organization.
Take Back Control with GridBeats™ APS
GridBeats™ APS is a single platform that simplifies software updates for protection and control devices — all without having to take them offline. It unbundles applications from hardware and helps reduce the number of devices needed in a substation.
Applied to aging infrastructure, GridBeats™ APS allows operators to run multiple P&C applications from just one device. This reduces the number of boxes in use across the grid and lets operators upgrade to new applications without having to overhaul any infrastructure.
Benefits for Operators:
• Standardizes control across legacy hardware to simplify complexity
• Automates patching and updates so old devices stay secure and consistent
• Keeps devices online and helps avoid planned outages to maintain aging assets
• Improves visibility across generations of equipment
• Creates a unified operational foundation that future-proofs today’s grid
• Enables modern tools, such as advanced monitoring, DER integration, and diagnostics
GridBeats™ APS lets operators modernize the grid and minimize the risks of aging technology. To see how it could work for your operation, visit our website.
This blog is the first part of a five-part series. Stay tuned to learn more about how GE Vernova's portfolio of solutions can help utilities modernize their grid networks.