A Simpler Path to Cyber Grid Resilience
The electric grid is in an era of change.
As utilities modernize infrastructure to integrate renewables, accommodate growing electricity demand, and improve operational flexibility, cybersecurity is becoming inseparable from grid operations. It's no longer a standalone function or compliance exercise—it is a foundational capability that enables a resilient, reliable, and intelligent grid.
The conversation around cybersecurity often begins with statistics1 about the growing volume and sophistication of cyber threats. Those numbers are important, but they only tell part of the story.
As discussed in my last blog, complexity due to the interconnected nature of the grid is one of the causes of increased cyber threats. Now, we’ll explore ways to help strengthen your grid’s cyber resilience in consideration of growing system complexity.
Complexity: A million entry points
Today’s grids are often a collage of aging and modern infrastructure, point solutions, and siloed data repositories. It’s a lot to manage.
Maintaining consistent cybersecurity across these environments can be difficult when operators are managing multiple device platforms, various firmware versions, disconnected software tools, and maintenance processes that often require planned outages. As grid networks continue to evolve, reducing operational complexity is becoming just as important as defending against external threats.
Cyber resilience requires a new operating model
Here’s the good news. The future of grid cybersecurity is not about adding more point solutions. It is about creating a simpler, more manageable operating environment.
That means giving utilities greater control to:
• Gain visibility across distributed substation assets
• Patch vulnerabilities in minutes, not days
• Consolidate systems into one, secure environment
• Upgrade devices with reduced downtime
• Proactively maintain and defend the grid
This shift enables utilities to spend less time managing infrastructure and more time operating a resilient grid.
The future, unbundled
One of the most promising developments is a new generation of a grid-specific, purpose-built platform that gives grid operators the edge in cyber defense.
In practice, this means that:
• Firmware can be updated remotely, without taking devices offline
• Operators can consolidate hundreds of communications and cybersecurity packages into standardized estates
• Security patches can be deployed consistently across multi-vendor environments
• Operators gain total visibility into device status, vulnerabilities, and update history — from anywhere
All adding up to a grid that’s easier to manage, more secure, and more flexible.
GridBeats™ APS: Giving operators back control
At GE Vernova, we believe the next generation of digital substations will be built around platforms that are easier to manage, easier to maintain, and simpler to secure.
This philosophy is reflected in GridBeats™ Automation and Protection System (APS), which is a single platform that simplifies software updates for protection and control (P&C) devices.
GridBeats™ APS lets operators unbundle core P&C functions from platform elements, so they can remotely update or patch platform firmware in minutes without needing to take devices offline. This keeps P&C devices secure, improving resilience and reliability and avoiding the costs of downtime.
And instead of having to potentially run hundreds of communications and cybersecurity packages, GridBeats™ APS lets you run as few as 10, all while maintaining the same level of control and protection.
The result is a simpler operational model that supports stronger cybersecurity, greater operational flexibility, and improved lifecycle management.
Building the resilient grid of tomorrow
As our industry continues its digital transformation, utilities have an opportunity to rethink how cybersecurity is integrated into grid operations, and not as an obstacle to modernization, but as an enabler of it.
The utilities that succeed will be those that simplify their operations through platforms such as GridBeats™ APS, while strengthening their ability to adapt. In an increasingly connected grid, resilience begins with control, and control begins with simplicity.
1 U.S. utilities experienced a near 40% surge in cyberattacks in 2025. In 2024, worldwide critical infrastructure was hit by over 420 million cyberattacks and 42% of critical infrastructure companies have been victim to a data breach.